Part Number: TM4C1294NCPDT
I am using the following:
ccs 6.1.2
TIRTOS 2.16.0.08,
compiler 5.2.7
XDC 3.31.1333
TM4C1294NCPDT
ndk_2_25_00_09
I would like to use TFTP to receive about 5M Bytes of data I need to write to a serial device so I need to receive a block of data write it to a serial device and get more data from TFTP till I have moved all 5 M Bytes.
Are there any examples I could leverage to see how to implement this?
I have found the following source that has some functions that look like they would help.:
C:\ccs6p1p2\tirtos_tivac_2_16_00_08\products\ndk_2_25_00_09\packages\ti\ndk\nettools\tftp
One example that could be leveraged possibly is the boot code in the Tiva since the boot code supports TFTP / BootP to do firmware update over Ethernet.
Where can I find the source code for the Tiva boot code and are there other examples of implementing a TFTP client using the functions in the code in the path above?
Thanks,
Doug