Other Parts Discussed in Thread: UNIFLASH
Hi Frank, hi TI
In the file of AM263x Lauterbach is burn_flash file. Hier in the am263x-S25FL128SA-qspi.cmm file is written, that the DIP switches need to be QSPI_1.

When I change the switches to QSPI_1s or QSP_1 Uart mode, then I cannot write on the flash. only Devbot allows me to right the flash.
Is that an expected behavior?
and how can I run the code from flash?
are there more steps after loading the code into flash?
Thank you in advance