Part Number: TMS570LC4357
Other Parts Discussed in Thread: UNIFLASH
Hi:
I have met the ECC broken error. In my project, we use .ld file as link file instead of .cmd. In this case, some syntax error occurd when I add these code below:
ECC_VEC (R) : origin=(0xf0400000 + (start(VECTORS) >> 3))
length=(size(VECTORS) >> 3)
ECC={algorithm=algoL2R5F021, input_range=VECTORS}
ECC {
algoL2R5F021 : address_mask = 0xfffffff8 /* Address Bits 31:3 */
hamming_mask = R4 /* Use R4/R5 build in Mask */
parity_mask = 0x0c /* Set which ECC bits are Even and Odd parity */
mirroring = F021 /* RM57Lx and TMS570LCx are build in F021 */
}
So do you have .ld file example of ECC?