Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG
Hi Team,
I am suffering from the capture interrupt.
I just want to capture the pulse width. The timing of the interrupt and the captured pulse width are both incorrect.
I think maybe it was because of my config that cause the problem. Then I use the SDK:‘timh_timer_mode_capture_edge_capture’ , and capture is wrong either.
I changed the TIMH0 to TIMA1. It failed. Is there any bug in MSPM0? Or is there any bug in those encapsulation function"DL_Timer_XXXXXXX" ?
So I went to see the reg . Refer to the TRM.

I found the IMASK is different from my debug.

And I try to change it by myself and failed.
It doesn't work.
I really really don't know what to do. It cost me a lot of time and I haven't made any progress.
I wish someone could help me to solve the problem.
Other reg is shown in the following figure.