This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507: Warning while configuring SYSPLL

Part Number: MSPM0G3507


When I use internal or external clock to source SYSPLL, I am getting below warning if the VCO is other than 160MHz.

Warning:

MSPM0G currently only includes internal parameters to support configuring fVCO at a recommended frequency of 160MHz. Pending characterization, other frequencies might result in reduced accuracy or the PLL locking onto a wrong frequency entirely

Is this some limitation? I am using 24MHz crystal in our breakout board. With this, there is no way for me to achieve 160MHz VCO.

Thanks & Regards

Vijaya