Other Parts Discussed in Thread: AM2434, , SYSCONFIG
Hello expert,
we have been developing our product on am2434 and we are switching to am2431,
till this day we have been using this software for development,
CCS v11.1
SDK v8.3
Sysconfig v1.12
If I understand it correctly to use the am2431 we need to upgrade to:
SDK v8.5
CCS v12.1
Sysconfig 1.14.
Launch procedure:
However when I want to create new target configuration I still only see AM2434_ALX in device types. When i select this
and select AM24x.gel for M3 core. And try to initialize with
loadJSFile C:\ti\mcu_plus_sdk_am243x_08_05_00_24\tools\ccs_load\am243x\load_dmsc.js
This produces error: Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings.
This procedure was previously working for the am2434.
So my questions are:
What is the required SKD, CCS and sysconfig version for AM2431_ALX?
When creating target configuration for AM2431_ALX. Do I need to do anything else than selecting the AM24x.gel file for M3 core?
Is the procedure for connecting to device different on AM2431 different then the one I have described above ?
Thanks for you help and have great day!
Dominik