Other Parts Discussed in Thread: HALCOGEN
Hello
Regarding the control of special multiplexed options for the temperature sensors selection:
1) Is the correct understanding for setting PINMMR174[24] = 1, it means that the temperature sensors are disabled, neither Temp Sensor 1/2/3, AD1IN[31], AD2IN[31] nor AD2IN[30] is usable or available (despite a possible setting as stated in SPNU563A "Table 6-11. Temperature Sensor Selection")?
2) But when using Temp Sensor 1/2/3, AD1IN[31], AD2IN[31] or AD2IN[30], PINMMR174[24] has to be 0 + corresponding setting as given in the table;
e.g. using Temp Sensor 2: PINMMR174[24] = 0 and AD2CHNSEL(31) = 1, PINMMR173(24) = 0, PINMMR173(25) = 1
Thanks in advance for your support
Mathieu