This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
1. The ESM interrupt "ESM_G1ERR_EPC_SERR" was not triggered after we use "SL_SelfTest_Flash" with passing test type "FLASH_ECC_TEST_MODE_1BIT" to insert EPC 1-Bit ECC error.
2. The ESM interrupt "ESM_G2ERR_EPC_UNCORR" was not triggered after we use "SL_SelfTest_Flash" with passing test type "FLASH_ECC_TEST_MODE_2BIT" to insert EPC ECC uncorrectable error.
Can you help please check if anything wrong in your diagnostic library code as below?
Have you tested all the APIs and verified their usability on RM57L843? If yes, can you help provide the test report for our reference. Thanks so much
Hi Shenruming,
Can you help please check if anything wrong in your diagnostic library code as below?
Have you tested all the APIs and verified their usability on RM57L843? If yes, can you help provide the test report for our reference.
There should not be anything wrong with diagnostic library code. Yes, they are all tested.
Let me test at my end update you.
--
Thanks & regards,
Jagadish.
Hi Jagadish,
1. Now, "FLASH_ECC_TEST_MODE_2BIT" error forcing test can generate ESM group2 interrupt "ESM_G2ERR_CR5_BUSERR" normally.
QJ said it's as expected. But in other post, you confirmed that "FLASH_ECC_TEST_MODE_2BIT" will trigger "ESM_G2ERR_EPC_UNCORR".
Can you check again which fault "FLASH_ECC_TEST_MODE_2BIT" will trigger?
2. "FLASH_ECC_TEST_MODE_1BIT" error forcing can generate ESM group1 interrupt "ESM_G1ERR_EPC_SERR" normally.
Hi Shenruming,
Apologies for the delay,
1. Now, "FLASH_ECC_TEST_MODE_2BIT" error forcing test can generate ESM group2 interrupt "ESM_G2ERR_CR5_BUSERR" normally.
QJ said it's as expected. But in other post, you confirmed that "FLASH_ECC_TEST_MODE_2BIT" will trigger "ESM_G2ERR_EPC_UNCORR".
Can you check again which fault "FLASH_ECC_TEST_MODE_2BIT" will trigger?
QJ was correct.
--
Thanks & regards,
Jagadish.