Hello,
I'm using early samples of the reference indicated
I have this message every time I launch the debugger, is there a way to not have this message, please?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm using early samples of the reference indicated
I have this message every time I launch the debugger, is there a way to not have this message, please?

Hi Thomas,
Please see this note [FAQ] Important note for Early MSPM0 Customers, I believe you are using the wrong version of the IDE.
Regards,
Luke
Hello Luke,
Seems so, thanks, I now have access to my secure ressources with the correct IDE and datasheet :) - let me try to install all that and play with it tomorrow
Thanks
Hello, I removed the last CCS and installed CCS 12.1.0 - according to the note from early samples SDK shall be max 0.58.00.00 but when I install CCS 12.1.0 it comes with SDK 1.00.00.4
I installed SDK0.58.00.00 but it doesn't appear in the ressource explorer
Over that the reference MSPM0G3507 is not known when I try to create a new project - I made a full installation of CCS 12.1.0
Any Idea what I shall try? Is there a recommended version of CCS that comes with the correct SDK for early samples, please?
Thanks
Let me try to follow this step by step:
Hope one day it will be one unique installer