Part Number: TM4C123GH6PM
Hello,
Is there a way to reformat the TM4C and delete the software flashed so that the device is how it originally was before it was programmed?
Thanks,
Seong
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C123GH6PM
Hello,
Is there a way to reformat the TM4C and delete the software flashed so that the device is how it originally was before it was programmed?
Thanks,
Seong
Hi Seong,
If you just erase flash you can do it in CCS. See below.

But if you want to fully restore the device to its factory settings then you need to do a unlock. t This is a mass-erase. The difference between unlock/mass-erase and erase is that mass-erase will also erase the on-chip EEprom and all non-volatile registers. See below if you are using a LaunchPad or ICDI as the debug probe. You can use LM flash programmer to unlock the device.

If you are using a debug probe such as XDS100 or XDS200 or XDS110 you can use dbgjtag.exe command to unlock. See section 5.3.2 in this app note for details.