Part Number: TMDS570LS31HDK
Other Parts Discussed in Thread: HALCOGEN
Hello,
I am trying to generate a CRC on Flash memory using the SL_CRC_Calculate() function. However, I cannot find a way to access the origin or start address of the .cinit section in memory. I know the linker provides the symbols __TI_CINIT_Base and __TI_CINIT_Limit, but this does not cover the whole .cinit section as can be seen from the map file:
SECTION ALLOCATION MAP
output attributes/
section page origin length input sections
-------- ---- ---------- ---------- ----------------
.kernelTEXT
* 0 00000020 00005604
00000020 00002f04 os_tasks.obj (.kernelTEXT)
00002f24 000012dc os_queue.obj (.kernelTEXT)
00004200 00000818 os_event_groups.obj (.kernelTEXT)
00004a18 000004b0 os_portasm.obj (.kernelTEXT)
00004ec8 000003e0 os_port.obj (.kernelTEXT)
000052a8 0000037c os_heap.obj (.kernelTEXT)
.cinit 0 00005628 000000e8
00005628 0000009d (.cinit..data.load) [load image, compression = lzss]
000056c5 00000003 --HOLE-- [fill = 0]
000056c8 0000000c (__TI_handler_table)
000056d4 00000009 (.cinit..kernelBSS.load) [load image, compression = lzss]
000056dd 00000003 --HOLE-- [fill = 0]
000056e0 00000008 (.cinit..bss.load) [load image, compression = zero_init]
000056e8 00000008 (.cinit..kernelHEAP.load) [load image, compression = zero_init]
000056f0 00000020 (__TI_cinit_table)
...
GLOBAL SYMBOLS: SORTED BY Symbol Address
address name
------- ----
00000000 resetEntry
....
0000560c vPortInitialiseBlocks
00005628 __TI_static_base__
000056c8 __TI_Handler_Table_Base
000056d4 __TI_Handler_Table_Limit
000056f0 __TI_CINIT_Base
00005710 __TI_CINIT_Limit
Notably, there's __TI_static_base__ and __TI_Handler_Table_Base in between the end of the previous section (ends @ 0x5628) and the __TI_CINIT_Base (0x56f0).
I wasn't able to find any documentation on __TI_static_base__, and couldn't find any confirmation that the Handler table will always appear before the Cinit table. Is there a way to capture the whole of the .cinit section?
Thank you!