This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: Eeprom Blank check causes excpetion/corruption of the sector

Part Number: TMS570LC4357

Hi,

We are using F021 Flash API Driver Libray to verify blank checks on EERPOM Sectors. We have a requirement to log the data in EEPROM when a GIO interrupt occurs as mentioned below:

//On Power-Up

// Initlize Flashj

//Erase sector 7 of EEPROM

//

//

// Code Executes

// Initialize RTOS and run threads

while(1)

{

}

// GIO Interrupt

void isr_handler(void)

{

//Verify Blank check on sector 7 at address 0xF0207000

// Call Fapi_StatusTypeFapi_doBlankCheck( )

// Log Data in sector 7 at address 0xF0207000.

} 

But on a few power cycles, we are seeing either sector 7 getting erased or getting a data abort exception.

If we comment out  Fapi_StatusTypeFapi_doBlankCheck( ) function call, we are not seeing any issue and the code works well for every power cycle. Please let if we are missing any configuration specifically for the Blank check to use.