Part Number: AM2432
Hello,
I'm trying to write my own Switch Implementation on the PRU. For this I have written assembler code to test sending and receiving data over Ethernet. Receiving works, but I can't get the PRU to send data. For both ways I am using the L1 FIFO and the R30/R31 Interface. In Register 0x300B 2068 I can clearly see the FIFO filling up, but it never gets emptied. I already tried setting TX_ENABLE manual after filling the FIFO, but it seems like TX_EN never gets asserted.
From the Refernce Manual I understand, that TX_EN is automatically set, when these conditions are met:
1. TX L1 FIFO not empty
2. Interpacket gap (IPG) timer expiration
3. RX_DV to TX_EN timer expiration
4. TX_EN compare timer expiration
As far as I can tell, all these Requirements are met, so I can't figure out, why the FIFO is not being emptied.
So here are a few questions that might get me further with my problem:
1. What are the minimal requirements for sending data to the MII? Do I need to send a valid frame or would some Bytes of 0xFF still get processed further? Do I need to configuere a MAC and MDIO?
2. Where can I read, if RX_DV or TX_EN is set? Where can I see if the above named timers are expired?

Also during my research I found this in the Refernce Manual on page 3261:
4.11.2.4.1.1.4.1 TX Preemption Programming Model
Start a new frame.
1. Wait until R31.TX_EOF event
2. Load data into TX L2 FIFO until the full frame is completed
3. Issue a R30.TX_EOF + TX_CRC_HIGH + TX_CRC_LOW
Shouldn't it be R31 instead of R30?
Thanks in advance for your answer.
Best regards
Marius Apostel