Part Number: MSPM0G1106
Hi!
I'm having a problem with the MSP0G.
I've alread had this problem with a PG1 unit, and the answer was to change to a PG2 microcontroller.
I've already have the NEW PG2, and as I understand, it is not really the 1106, the unit that TI sent was an 3507 but being a 32 pins unit, with the same layout as the 1106.
The main problem is that after 10 seconds of the code to start running, it is being sent to the Default_Handler witn an Exception 011b, which is the HardFault_Handler.


I am currently running:
- Systick
- 2 free running timers (TIMA1 and TIMG6).
- Two I2C Channels:
- Multimaster mode with interruption.
- Master mode with polling to an EEPROM.
- TIMG0 as a 10 ms timer with interruption.
- PWM TIMG12.
- Compare timer ( 16 edge counter ) TIMA0 with interruption.
Sincerely I don't know what to do.
I'll appreciate your help