Part Number: AM2434
Hello:
A problem was encountered when using the gpio interrupt example.
The original example works fine, but after modifying the gpio pin from C13 to W6, the program does not run, with the following error
"[MAIN_Cortex_R5_0_0] [Error] Sciclient event config failed!!!
ASSERT: 0.12333s: syscfg/ti_drivers_config.c:Sciclient_gpioIrqSet:116: FALSE failed !!!"
===================================================================
Development board:AM243xEVM
Example:gpio_input_interrupt_am243x-evm_r5fss0-0_nortos
SDK: mcu_plus_sdk_am243x_08_06_00_43
help me ,thanks