Part Number: SIMPLELINK-MSP432-SDK
Hi
I was hoping someone could answer my question regarding the TI Code Composer Studio and MPS432-SDK software
The software is added to our lab image where students are using the MSP432 board.
I believe i installed the SDK software successfully after installed the TI CCS software. However, there seems to be additional manual steps to make use of it once a new profile logs into the Windows computer.
How can this be avoided or corrected during the installation phase?
Prior to image capture, if I sign in under the profile and do this step manually, do these changes get applied to the Default User so that any new user that signs in will adopt this automatically?
thank you,