This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team
There's an issue from the customer need your help:
When updating XDS110, I accidentally pulled the cable, and as a result, I couldn't connect it, and I couldn't program it
So I read the XDS110SupportReadMe .pdf, followed what it said, and found that I could find the device and enter DFU mode
But when rewriting the firmware .bin, I can't open the file (I can make sure that the USCIF folder has this thing and the name is correct)
I've also tried it on other people's computers, and they all can't open the file in the same way.
I've tried downloading the new firmware .bin and it still doesn't open
I don't know why I can't get down, is the debugger broken, but I can obviously connect it.
Thanks & Regards,
Ben
Hello,
When updating XDS110, I accidentally pulled the cable, and as a result, I couldn't connect it, and I couldn't program it
Disconnecting the cable during the firmware update process would cause a failure and likely corrupted firmware on the XDS110.
But when rewriting the firmware .bin, I can't open the file (I can make sure that the USCIF folder has this thing and the name is correct)
The current directory is "C:\Users\Think" and not the xds110 directory. So you would need to provide the full path to firmware.bin, not just the file name.
Thanks
ki