Part Number: AM2634
Hello,
I have HSM software and need to integrate it inside the SBL, is there any guide for this?
Yours,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM2634
Hello,
I have HSM software and need to integrate it inside the SBL, is there any guide for this?
Yours,
Hi Abdelrhman Afifi,
The HSM firmware integration is already covered as part of SBL for HS-FS devices as mentioned below - https://software-dl.ti.com/mcu-plus-sdk/esd/AM263X/latest/exports/docs/api_guide_am263x/SECURITY_PAGE.html
If you need more insights on integration and enablement of Security on AM263x devices, please refer to AM26x MCU+ Academy - "Enabling Security" --
https://dev.ti.com/tirex/explore/node?node=A__AESgmqK3b93425uf.HP2zA__AM26X-ACADEMY__t0CaxbG__LATEST
Best Regards,
Aakash
Thanks for your help,
I have a follow-up question If the board SBL load the HSM firmware and then the SBL jumps to my application, my application needs to use the HSM firmware.
Is it required to load it again inside the application or is it just loaded once in the board SBL?
Yours
Hi Abdelrhman Afifi,

As per the secure boot flow, the SBL is responsible for HSM Run Time. After the HSM Run Time is loaded, SBL or Application can leverage the same.
This will inform about the same - https://software-dl.ti.com/mcu-plus-sdk/esd/AM263X/latest/exports/docs/api_guide_am263x/EXAMPLES_HSM_SERVICES.html#autotoc_md1575
Best Regards,
Aakash
Hello,
What are the types of reset that will require HSM firmware reloading? (i.e. power-on reset, warm reset,....)
Does resetting the Host core will reset the HSM core as well?
After conversion to SE, it is mentioned that the debug port will be disabled, how should I test and debug my software?
Hi Abdelrhman Afifi,
By default the debug access to HSM as well as public cores are disabled in case of HS-SE devices. The request can be requested via HSM Client service as mentioned here - https://software-dl.ti.com/mcu-plus-sdk/esd/AM263X/latest/exports/docs/api_guide_am263x/EXAMPLES_HSM_SERVICES.html
More details in My Secure SW link here - https://software-dl.ti.com/secure/software/sitara-sec/AM263X-RESTRICTED-SECURITY/TIFS_MCU/v08_06/tifs_am263x_08_06_00_05_docs_only/docs/api_guide_am263x/html/HSM_DBG_SRV.html?__gda__=1691584887_6db356badf79dfd78f25461319c0c8dd
Hope it helps.
Best Regards,
Aakash
Hi,
What are the types of reset that will require HSM firmware reloading? (i.e. power-on reset, warm reset,....)
In terms of reset, there are warm reset and cold reset(PORZ). For either of the cases the HSM needs to be reloaded.
Does resetting the Host core will reset the HSM core as well?
If you mean by FSM trigger, it only resets the subsystem. It has no impact on SoC, hence no impact on HSM core as well.
Best Regards,
Aakash
Hi Aakash,
Thanks for your help.
If the SBL loads the HSM and then gives control to the application, what are the required APIs the application should call in order to use the HSM?
The application does not need to reload the firmware again, but does it need to call the init API for example?
Hi Abdelrhman Afifi,
what are the required APIs the application should call in order to use the HSM?
All the mentioned APIs in the HSM Client details are explained in the link above.
The application does not need to reload the firmware again, but does it need to call the init API for example?
HSM will be initialized during its installation. Application can directly invoke client APIs to use HSM Services. Client Init at application end will be handled via System_Init code generated as part of syscfg.
Hope it helps.
Best Regards,
Aakash
Hello,
Client Init at application end will be handled via System_Init code generated as part of syscfg.
I am not using the SDK so the is no code to be generated from the syscfg.
So the needed API to be called in the Application before using HSM services is Client init? Is that correct?
So the needed API to be called in the Application before using HSM services is Client init? Is that correct?
That is the correct understanding.