Part Number: MSPM0L1303
Other Parts Discussed in Thread: SYSCONFIG, UNIFLASH
I did the same thing as this guy: disable the SWD pin, and lose programming access to the MCU
So there is still no way to recover the MCU if I do not have bootloader and disable SWD access from the start?
As I have limited board to play with, I think Yuhao Zhao's number 2 solution sounds pretty great.(add a delay before disabling SWD access)
Could you please help me to check that this is the correct thing to do, or is there anything i missed?:
1. in sysconfig, leave the "Debug Enable On SWD Pins" ticked. do not initialize the intended gpio pin
2. in main, use delay_cycles(??) to delay for a few second
3. use code below to disable debug
SYSCTL->SOCLOCK.SWDCFG = (SYSCTL_SWDCFG_KEY_VALUE | SYSCTL_SWDCFG_DISABLE_TRUE);
4. initialize the intended gpio pin
Thank you very much