This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I did the same thing as this guy: disable the SWD pin, and lose programming access to the MCU
So there is still no way to recover the MCU if I do not have bootloader and disable SWD access from the start?
As I have limited board to play with, I think Yuhao Zhao's number 2 solution sounds pretty great.(add a delay before disabling SWD access)
Could you please help me to check that this is the correct thing to do, or is there anything i missed?:
1. in sysconfig, leave the "Debug Enable On SWD Pins" ticked. do not initialize the intended gpio pin
2. in main, use delay_cycles(??) to delay for a few second
3. use code below to disable debug
SYSCTL->SOCLOCK.SWDCFG = (SYSCTL_SWDCFG_KEY_VALUE | SYSCTL_SWDCFG_DISABLE_TRUE);
4. initialize the intended gpio pin
Thank you very much
neither uniflash nor debugging using CCS works, when SWD is disabled in code + hold NRST low
but if I hold nrst low, connect to CS_DAP_0 core, and use FactoryReset_Manual DAP script, it will allow me to program the next time i try. i wander if there is a way to do this with uniflash only. i will ask this in a separate thread.
Hi Xiao,
Internally I am asking our SW team to look into this as well.
Just to reiterate section 27.1.2 in the TRM:
Hi Xiao,
I'm being told the device must go through a POR with the NRST held low in order to gain access to these pins. Uniflash cannot do this on its own.