This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5891-Q1 drive 60x60 LED matrix

Hi Ti experts,


If I want to light up a 60x60 LED matrix, how many ICs should I use, and how should I configure it in the demo code?

Do you have an example code for cascading multiple units?

  • Hi Allen,

    please provide the below information which are necessary:

    1. 60 * 60 LED Matrix means RGB LED or monochrome LED?
    2. how much average current do you need?
    3. do you have any request about frame rate and refresh rate?

    it seems to be automotive application, it's a real project or study project? do you have any schedule?

    if the information needs to be confidential, you can send to my email(monet-xu@ti.com). thanks!

    BR

    Monet Xu