Part Number: TMS570LS3137
Hello everyone! I have a doubt about my bootloader program. The program is working fine. I was able to record a simple program. But now, I want to record another program, that uses FreeRTOS. I generated the .bin and modified the sys_link, and then I recorded this new program with FreeRTOS. But when I want to run the new program with FreeRTOS, the bootloader always enters in the section: svcEntry b svcEntry I really need help with this issue. I don't know what I can do to fix it.
I copied the sys_link.cmd from my FreeRTOS program:
-retain="*(.intvecs)"
/* USER CODE BEGIN (1) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Memory Map */
MEMORY
{
VECTORS (X) : origin=0x00020020 length=0x00000020
FLASH_CODE (RX) : origin=0x00020040 length=0x008000-0x40 fill=0xFFFFFFFF
FLASH0 (RX) : origin=0x00028000 length=0x0014FFC0
FLASH1 (RX) : origin=0x00180000 length=0x00180000
STACKS (RW) : origin=0x08000000 length=0x00000800
KRAM (RW) : origin=0x08000800 length=0x00000800
RAM (RW) : origin=(0x08000800+0x00000800) length=(0x0003F800 - 0x00000800)
/* USER CODE BEGIN (2) */
/* USER CODE END */
}
/* USER CODE BEGIN (3) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Section Configuration */
SECTIONS
{
.intvecs : {} > VECTORS
/* FreeRTOS Kernel in protected region of Flash */
.kernelTEXT : {} > FLASH0 | FLASH1
.cinit : {} > FLASH0 | FLASH1
.pinit : {} > FLASH0 | FLASH1
/* Rest of code to user mode flash region */
.text : {} > FLASH0 | FLASH1
.const : {} > FLASH0 | FLASH1
/* FreeRTOS Kernel data in protected region of RAM */
.kernelBSS : {} > KRAM
.kernelHEAP : {} > RAM
.bss : {} > RAM
.data : {} > RAM
}
Thank you so much.