Part Number: TMS570LC4357
Other Parts Discussed in Thread: TMS570LS3137
Hello,
I am seeing the exact problem raised in the below link except that the controller P/N is TMS570LS3137 and I don't see any solution provided in the link.
I have configured SCI-1(Multi-buffered, 8 bytes) for both RX and TX DMA. DMA CH-0 is for RX and DMA CH-1 for TX with AIM mode set to FALSE. I am trying to transfer 4 frames of 8 bytes with 2 elements (32_bit transfer) in each frame.
Is it that the SCI TX DMA always getting triggered leaving no room for RX DMA despite priority is high for Rx DMA channel?
I even tried with low priority for TX DMA CH-1 but it didn't work either. Also, I was expecting the DMA CH-1 will get disabled after a block transfer of 32 bytes (4 frames of 8 bytes) but it is always enabled.
Any help?
Thanks,
Jai