Other Parts Discussed in Thread: TMS570LC4357
Hello,
I got a prefetch abort exception on my TMS570LC4357 MPU. In the Cortex -R5 Revision: r1p2 Technical Reference Manual I found the “Instruction Fault Address Register” (IFAR). I added the code line MRC p15, #0, R0, c6, c0, #2 in order to read the instruction, that caused the prefetch abort. From the IFAR I got the address 0xFF278E68.
But that didn’t helped because the area is completely zero. According to the Technical Reference Manual, it should be between these two addresses:
DCAN1 RAM ECC 0xFF1E0000 0xFF1FFFFF
MIBADC2 RAM Parity 0xFF3A0000 0xFF3BFFFF
Did I read the register correctly?
Some more infos:
The HW and SW is tested the whole time with the same test in a loop.
The prefetch abort occurs after various time. For example (sometimes after a 40 minutes run, 1 hour run …)
Does someone have an idea how to locate the problem?
Thanks for any help!