hello, we use j721s2 rtos sdk 08_06_00, sbl boot mode, mcu1_0 run autosar, which demo can be refer to use cddipc communicate to linux ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello, we use j721s2 rtos sdk 08_06_00, sbl boot mode, mcu1_0 run autosar, which demo can be refer to use cddipc communicate to linux ?
Hello,
Thanks for writing to us. CDD IPC to communicate with Linux for mcu1_0 the current examples are not working as expected and internal ticket is also raised to fix this issue.It is will be part of upcoming SDK version 9.1.Sorry for the inconvenience.Only the examples have limitation driver files will work as expected.
CDD IPC app linux is currently working on J721E platform.
Regards
Tarun Mukesh
Hello,
we don't currently have working demo for you to show the communication with A72 from any R5 core in J721S2 MCAL.You can refer the FAQ
In MCAL, it is going to be part of next SDK version only for j721s2. MCAL-12861 is the internal ticket
Regards
Tarun Mukesh