Part Number: TM4C129XNCZAD
I'm using the emWin graphics library. It has a small number of configuration files that are specific to the given hardware and display. I either have to generate a emWin library that includes these configuration files - which will be different for each target hardware, or its documentation states that I can include all of the emWin files in a given CCS project if the linker is a "smart linker" that will only link in the object files that are used and not all of the libraries object files.
CCS version 10.4.00006. Does the linker have this ability? Are there any link flags that need to be set?
Thanks, Doug