Other Parts Discussed in Thread: EK-TM4C1294XL
Hi,
We have bunch of devices installed over local network. We have used the remote programming approach using LM Flash Programmer and it works fine. However one thing we have noticed, the programmer would take 5-8 minutes to discover the remote device once it finds the remote device the programming takes less than a minute. We have couple of switches in the network. However we have also tried a small Local network where only the TM4C MicroController was connected but the LM Flash programmer would still take around 4-5 minutes to discover it.
I have following question;
- Is this a known issue ? Any idea what could be causing it ? Alternatively, how can I speed up to discover the remote device faster
- Since we have bunch of devices installed on the network, it is very tedious and manual work to enter MAC address for each device. Is there any way I write a python script which would hold bunch of MAC addresses that will be fed to the LM Flash Programmer and the programmer will start programming the device one after the other ?
- Is there Linux version (Redhat) for LM Flash Programmer ?
Thanks