Part Number: MCU-PLUS-SDK-AM243X
Other Parts Discussed in Thread: LP-AM243
I built the demo below and checked its operation.
"ethernetip_adapter_generic_device_mii_demo_am243x-lp_r5fss0-0_freertos_ti-arm-clang"
We checked with version 09.00.00.03 of INDUSTRIAL-COMMUNICATIONS-SDK-AM243X.
We then conducted a CT19.1 protocol test on these.
At that time, the following error occurred in LLDP Management Object Test.
1323 1> *** The required System Capbility TLV is missing.
1324 2> *** The required Management Address TLV is missing.
1325 3> *** The required CIP Identification TLV is missing.
1326 Found 62 padding bytes in the frame.
1327 01 80 C2 00 00 0E 1C 63 49 25 1D CC 88 CC 02 07 04 1C 63 49 25 1D CC 04 07 05
1328 50 6F 72 74 20 31 06 02 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
1329 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
1330 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
1331 Received a valid LLDP frame.
1332 4> *** Still received a LLDP frame after LLDP disabled.
Although it is a shutdown LLDP frame, it seems that the packet size remains unchanged at 100 bytes.
When I checked the Known Issues, I found the following issues.
[DTKEIPA-1838]
Sporadic LLDP error reported by CT19.1 after changing msgTxInterval.
The ODVA Conformance Test sets the LLDP msgTxInterval (Instance Attribute 2 in LLDP Management Object) to 5 seconds. After that the DUT correctly transmits a LLDP frame immediately (see IEEE802.1 chapter 9.2.10 Transmit timer state machine). The subsequent LLDP frame is occasionally not send correctly after 5 seconds.
Is the above error related to Known Issues?
Also, will it be fixed in the next release?