The previous thread got locked, so I'll ask here.
I built the demo below and checked its operation.
"ethernetip_adapter_generic_device_mii_demo_am243x-lp_r5fss0-0_freertos_ti-arm-clang"
We checked with new version 09.01.00.03 of INDUSTRIAL-COMMUNICATIONS-SDK-AM243X.
However, the following auto-negotiation failure symptoms continue to occur.
When the other party to connect to is forced 100Mbps half-duplex, the link is up, but the values of the following objects are incorrect.
"Ethernet Link Object - Instance 1 - Attribute 2: Interface Flags"
As shown below, Ethernet Link Object - Instance 1 - Attribute 2: Interface Flags's Bit1 was set to 1, indicating that the link was up in full duplex mode.

Link status when auto negotiation fails_ind_comms_sdk_am243x_09_01_00_03.zip
Could you confirm this phenomenon again?