Part Number: AM2432
Other Parts Discussed in Thread: UNIFLASH, , AM2434
We have a custom board using AM2432B (ALX package). I am attempting to bring it up and am running into some issues.
I attempted to perform SoC flash initialization utilizing the uart_uniflash.py and the am243x-lp default_sbl_null.cfg; however, I get stuck on the second step. I have verified the device type as HSFS and am using the hs_fs images.
I wonder if this is because the ROM code is expecting a signed SBL image with board configuration info specific to the AM2432 (ALX Package) rather then the AM2434 (ALX Package) which is used on the am243x-lp.

Do I need to rebuild the SBL with a different board config or is there something else going on here?
Any assistance is greatly appreciated.
Thanks,
Dan