Part Number: RM57L843
Hi team,
I am using RM57l843 microcontroller, I am studied the TRM page no. 854, section 22.2.2.2.2.2 Example ADC Conversion Sequence using Enhanced Channel Selection mode. If Enhanced Channel Selection mode means For example channel 5,4,8,2 are selected for conversion. In sequential conversion mode the channels are converted in ascending order of channel 2,4,5,8. But In Enhanced Channel Selection mode the channels are user defined selection the conversion order is 4,5,8,2 or 2,8,4,5. Is my understanding is correct or not?
I don't know I am understand correct or not about the Enhanced Channel Selection mode. I have doubts on External 5-bit and Internal 5-biT, LUT.
And If I my assumption is correct means then How to configure to select channel 8 is convert first and 4,5,2.
Thanks,
Regards,
Veerappan P A