Other Parts Discussed in Thread: SYSBIOS
I am trying to use a capture control pin to measure the PWM of a input pin. I have read around and found that this is easiest using 2 pins, but sadly only have 1 on my current application. I'm using T0CCP0 to use timer 0A interrupt. The code looks like this:
application.cfg setup to create HWI and switch internal clock to use timer3
var Clock = xdc.useModule('ti.sysbios.knl.Clock');
Clock.timerId = 3; /* use timer 3 */
var ti_sysbios_family_arm_m3_Hwi3Params = new ti_sysbios_family_arm_m3_Hwi.Params();
ti_sysbios_family_arm_m3_Hwi3Params.instance.name = "motorSpeedIntHandle";
Program.global.motorSpeedIntHandle = ti_sysbios_family_arm_m3_Hwi.create(19, "&MotorSpeedIntHandler", ti_sysbios_family_arm_m3_Hwi3Params);
pwm_measure.cc
extern "C" void MotorSpeedIntHandler() {
static uint32_t pwm_fall_edge = 0;
static uint32_t pwm_rise_edge = 0;
static uint32_t log_counter = 0;
// Timer has timed out
if (TimerIntStatus(TIMER0_BASE, TIMER_TIMA_TIMEOUT) == TIMER_TIMA_TIMEOUT) {
// If we timed out throw away sample
pwm_fall_edge = 0;
pwm_rise_edge = 0;
TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
}
if (TimerIntStatus(TIMER0_BASE, TIMER_TIMA_TIMEOUT) == TIMER_CAPA_EVENT) {
int32_t pin_value = GPIOPinRead(GPIO_PORTL_BASE, GPIO_PIN_4);
if (pin_value == 0) {
pwm_fall_edge = TimerValueGet(TIMER0_BASE, TIMER_A);
int32_t pwm_on_time = pwm_rise_edge - pwm_fall_edge;
motor_speed_measured_RPM = (pwm_on_time / MOTOR_PWM_FEEDBACK_SPEED_CONVERSION_INVERSE);
} else {
pwm_rise_edge = TimerValueGet(TIMER0_BASE, TIMER_A);
}
TimerIntClear(TIMER0_BASE, TIMER_CAPA_EVENT);
}
}
void motorControlFeedbackInit() {
// Signal is a 482Hz from 5% - 100% duty cycle
SysCtlPeripheralDisable(SYSCTL_PERIPH_TIMER0);
SysCtlPeripheralReset(SYSCTL_PERIPH_TIMER0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
// Initialize timer A and B to count up in edge time mode
TimerConfigure(TIMER0_BASE, (TIMER_CFG_SPLIT_PAIR | TIMER_CFG_A_CAP_TIME | TIMER_CFG_A_ACT_NONE));
// 120MHz / 4 = 30MHz
TimerPrescaleSet(TIMER0_BASE, TIMER_A, 4);
// Timer a records pos edge time and Timer b records neg edge time
TimerControlEvent(TIMER0_BASE, TIMER_A, TIMER_EVENT_BOTH_EDGES);
TimerLoadSet(TIMER0_BASE, TIMER_A, 0xFFFF);
//Configure the pin that the timer reads from (PL4)
GPIOPinConfigure(GPIO_PL4_T0CCP0);
GPIOPinTypeTimer(GPIO_PORTL_BASE, GPIO_PIN_4);
TimerIntRegister(TIMER0_BASE, TIMER_A, MotorSpeedIntHandler);
// Enable the indicated timer interrupt source.
TimerIntClear(TIMER0_BASE, (TIMER_CAPA_EVENT | TIMER_TIMA_TIMEOUT));
TimerIntEnable(TIMER0_BASE, (TIMER_CAPA_EVENT | TIMER_TIMA_TIMEOUT));
TimerEnable(TIMER0_BASE, TIMER_A);
}
The problem I'm having, is as you see in the init function, I manually register an interrupt because it wasn't working through the .cfg once I register this interrupt(or unregister whatever one is already set) the RTOS crashes. I suspect that this is because the RTOS is using timer0 that it's doing something behind the scenes that registers it's own tick interrupt and doesn't like when I try to overwrite that. Am I missing something in the .cfg?
Thanks!