This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: QUADRATURE PULSE GENERATOR

Part Number: TMS570LC4357

sir  i  need using  capture register  will be  able  to find  frequency , then  value   present  in  that  register it will be  micro , milli , nano sec  that   information ,i need it ,  and  in PWM calculate time period we one formula  time period = period (ns) * clock frequency (Mhz) -1  like is they any formula for quadrature capture period register.

please as soon as possible,

thank you,

nanda kumar

  • Hi Nanda Kumar,

    The capture timer will run from the prescaled VCLK3.

    For example if your VCK3 is 75Mhz.

    And your prescaled value is 2

    And if you got the capture register value of 500 then you should calculate the period like below

    Period = (1/(VCLK3/Prescaled_value))*Capture register value

    Period = (1/(75Mhz/2))*500

    Period = (1/37.5Mhz)*500 = 13.33uSec.

    In this way you should calculate the period.

    --
    Thanks & regards,
    Jagadish.