Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: UART Boot Mode port ID configuration via PIN?

Part Number: AM2434

In the data book "AM64x /AM243x Processors Silicon Revision 2.0", Table 4-4 and 4-5 (Primary and Backup Boot Mode Selection) show no port ID configuration for the UART interface. In Table 4-46 "UART Boot Parameter Table", however, "From Pins, Physical port number" is specified for the byte offset 264. Will a port configuration via PINs possibly be supported in future revisions? A pull up/down configuration on the currently reserved PINs would then have an effect.