Dear support forum,
regarding the emulated EEPROM inside the TMS570LS family, we might face issues regarding the timing requirements:

The worst case time for a sectore erase of 8 s is simply to high.
Therefore, we think about "overwriting" the sector instead of erasing it and also store information of the memory position at which the important / new information starts.
=> The first question would be if this is possible or if a sector needs to be erased before being programmes again / overwritten.
=> The second question would be if erase of one sector and writing of another sector inside the BANK7 emulated EEPROM is possible. For BANKS this seems to be possible, but I am not sure regarding the sectors inside a bank.
Kind regards
Sebastian