Part Number: MCU-PLUS-SDK-AM243X
Hello
We are planning to have the possibility to run our device also without Industrial Ethernet protocol, so both Ethernet ports should run as "normal" IP ports (LWIP stack).
For this I still want to use the ICSS-EMAC, PRU-ICSS driver, but then I also have to use an Ethernet protocol. Can it cause problems if I use Ethernet IP for this? It seems to work for me.
I pass the "PRUSS_INTC_INITDATA_EIP" to the PRU-ICSS driver and use the library "ethernetip_adapter_mii_icss_fwhal.am243x.r5f.ti-arm-clang.release.lib".
Is there a firmware for the PRU-ICSS (Similar to that “ethernetip_adapter_pru0_bin.h”), if I only want to run the LWIP stack on the device?
Thanks for your help and best regards
Sebastian