This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM57L843: UART_Bootlader_RM57 Reset Function Questions

Part Number: RM57L843


Hi, TI team.

Hercules_Ethernet_Bootloader_RM57.zip
UART_Bootloader_LC4357_New.zip

UART_Bootlader_RM57.zip, which is a combination of the two bootloaders above, works well.

I have no problem using a serial bootloader, creating an application for the bootloader and getting it to work.

Question here.

I want to reset the application to software and run it from bootloader first.

Is there a way to do this?

When I jump to address 0, the bootloader starts and then freezes.
How can I reset to software?

Best Regards,

WBLee