This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Trying to debug MCBTMS570 Eval board with Blackhawk USB100v2 debugger



Hy,

I am trying to develop with the MCBTMS570 eval board from Keil. Debugging via the direct USB debugger on board is possible but very slow.
So now I am trying to get the Blackhawk USBv100v2 to work.

I followed this quick start guide: http://www.blackhawk-dsp.com/downloads/docs/guides/USB100v2-QS-01.pdf
Datasheet and quickstart guide for this and similar products can be found on: http://www.blackhawk-dsp.com/support/Docs.aspx#BH-USB-100

As the product I got was delivered with the quick start guide for USB100v2 (and 'not' model D)  I suppose I have this one.
But it doesn't really matter as the quick start guide is quite the same.

I am trying to get a debug conntection and this fails completely. So I think the problem is probably in the target device configuration. Which is all in Step 4 of the quick start guide.

Drivers:
I installed CCS4 and I am 100% sure I did it before I connecte the debugger as it is suggested in the manual.
I think the emulation driver from FTDI are installed successfully, as I get the device twice in the windows device manager as TI XDS100 Channel A and B.

Hardware installation:
I am 100% sure I attached the connectors in the corredt order since the first timer of connecting.

Any tipps how to configure this different to get a debug connenction?

 

Thanks

Florain

  • Florian,

    Just to be clear, you are trying to connect using CCS4 and not Keil uVision, correct? And the onboard XDS100v2 on the MDK works fine?

    >>I am trying to get a debug conntection and this fails completely. So I think the problem is probably in the target device configuration. Which is all in Step 4 of the quick start guide.

    What kind of a failure are you seeing?

    Regards,

    Abhishek

  • Hi Florian,

    The USB emulator on the Keil MCBTMS570 is an XDS100v2,  it's just embedded onto the board.

    So:

      - you should be able to use the same driver and configuration for the on-board XDS100v2 as for the standalone XDS100v2.

      - unfortunately, you'll get the same performance.

    There are a few things you can try in the configuration of CCS to speed up the XDS100v2.   You might try:

       1) choosing adaptive clocking and setting a max clock more like 3MHz for TCK (vs. default 1MHz)

       2) change your CCS option under Tools->On Chip Flash,  Erase Flash,  From "Entire Flash" to "Necessary Sectors Only".

           if you're just doing small programming examples then this will speed things up when you reprogram.   The TMS570 has a very large on chip flash (2MBytes) so it can take a long time if you always erase the whole flash but only needed to erase a few 100K bytes.

    But, the xds100v2 is really an evaluation tool - you should probably step up to a more powerful and faster emulator for serious work.

    Best Regards,

    Anthony

  • Hello Abhishek,

    I am using CCS4 but including the automated updates. I did hope, that the Debugger would speed up debugging, but as the next post answers it won`t(I will answer this extra).  At the momemt I am not definitely  which error code I am getting, but it's about that I am not getting any connection.
    Thanks so far!
    Florian

  • Hello Anthony,

    I thought something like that as it is working with the target device XDS100v2. Anyway I didn't order this debugger I just have no other tool at the moment. One question to
    '-unfortunately, you'll get the same performance':

    If there is the same harware on the Keil board as the XDS100v2. Means that this includes the same FTDI IC? Depending on IC I suggest this mainly slowes the speed of the connection, so the fast JTAG connection would be quite useless here.
    Am I right?

    But I think its still strange why the external Blackhawk is not getting a connection. Or is there something with the MCBTMS570 JTAG connection I missed?

    Anyway I thank you for the good tipps for debugging.


    But I couldn't follow the two of your following steps:

      1) choosing adaptive clocking and setting a max clock more like 3MHz for TCK (vs. default 1MHz)

       2) change your CCS option under Tools->On Chip Flash,  Erase Flash,  From "Entire Flash" to "Necessary Sectors Only".

    If it matters I have CCS  4.1.3.00038.
    If I am just blind please just write out your steps more precisely.

    Thanks!
    Florian

  • Another question Anthony,

    maybe there is a possibility that I get another Debugger. Can you recommend some. I think I read a list of debuggers in this forum some time ago.

    But I would like to know of someone who is working successful with it. So I have a feedback.

    Thanks

    Florian

  • Florian,

    you can find some information here and here.

    I know more 3rd parties support our devices than listed above and we are working on updating our product/wiki pages with that information.

    Regards,

    Abhishek