Hy,
I am trying to develop with the MCBTMS570 eval board from Keil. Debugging via the direct USB debugger on board is possible but very slow.
So now I am trying to get the Blackhawk USBv100v2 to work.
I followed this quick start guide: http://www.blackhawk-dsp.com/downloads/docs/guides/USB100v2-QS-01.pdf
Datasheet and quickstart guide for this and similar products can be found on: http://www.blackhawk-dsp.com/support/Docs.aspx#BH-USB-100
As the product I got was delivered with the quick start guide for USB100v2 (and 'not' model D) I suppose I have this one.
But it doesn't really matter as the quick start guide is quite the same.
I am trying to get a debug conntection and this fails completely. So I think the problem is probably in the target device configuration. Which is all in Step 4 of the quick start guide.
Drivers:
I installed CCS4 and I am 100% sure I did it before I connecte the debugger as it is suggested in the manual.
I think the emulation driver from FTDI are installed successfully, as I get the device twice in the windows device manager as TI XDS100 Channel A and B.
Hardware installation:
I am 100% sure I attached the connectors in the corredt order since the first timer of connecting.
Any tipps how to configure this different to get a debug connenction?
Thanks
Florain