Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG
Question regarding: MSPM0G3507

We need
-a. TIMA0 CCP0 85KHz and 50 percent duty cycle with risedelay on 1st output pin.
-b. The complement of a. but with risedelay on 2nd output pin.
- c. TIMA1 CCP0 synchronous, 50 percent duty cycle and phase shifted 0...180 degrees compared to a. risedelay at rising edge on 3th output pin.
-d. The complement of c. but with risedelay at rising edge 4th output pin.
I see that using edge aligned or center aligned PWM, it is possible to output the complementary pair with dead bands (next pictures).