Part Number: MSPM0G3507
Tool/software:
Hi TI Team.
I am working on MSPM0g3507 controller with interfacing i2c sensors those are SHT35 and HS300, before taking data from that sensor I want to probe and check if the sensor is present or not,
I have set the sensor addresses as 0x45 and 0x44 respectively.
i need to write the address and read the ACK from the sensor. so which driver function should I use that can capture and return ACK
so can use that ACK for probing sensor presence?
regards
Prajesh karmalkar