Part Number: MCU-PLUS-SDK-AM243X
Other Parts Discussed in Thread: UNIFLASH
Hi experts,
I have an question to consult.
Because current MX25LM25645G can only used with SPI mode but not OSPI mode. The related problem refer to PLUS-SDK-AM243X: 2434 EVM OSPI FLASH DIAG error
In this case, I can only use CCS to debug APP. When I download BOOT & APP through default_sbl_ospi.cfg, APP failed to load in BOOT(sbl_ospi project, see the below code).
For SBL_OSPI, I tried to modify flash config to SPI MODE and rebuild. And for default_sbl_osip.cfg, I tried to comment out the last line(... operation=flash-xip). But problem remain.
How do I need to modify the SBL_OSPI project and the default_sbl_ospi.cfg file?
int main(void)
{
...
bootHandle = Bootloader_open(CONFIG_BOOTLOADER_FLASH0, &bootParams);
if (bootHandle != NULL)
{
/* @Error:This function blocking forever */
status = Bootloader_parseMultiCoreAppImage(bootHandle, &bootImageInfo);
...
}
...
}