This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] MCU-PLUS-SDK-AM243X: [FAQ] How to debug/develop/migrate the flash driver for custom flash on non-TI EVM (OSPI/xSPI) ?

Part Number: MCU-PLUS-SDK-AM243X
Other Parts Discussed in Thread: UNIFLASH

  • I am facing issues while migrating the flash driver for custom flash.
  • The flash does not work out of the box with the steps mentioned.
  • How to debug the issues and I am new to the external flash environment ?
  • Why is my UART Uniflash not working on my board ? Why is my JTAG Uniflash not working on my board ?
  • Introduction

    AM243x is a System on Chip with a support of external flash. Customers are free to choose their custom flash. There are real challenges while integrating a custom flash. This FAQ will cover the problems faced during the SW configuration with AM243x device which has an xSPI controller.

    Note: AM243x supports different flashes for different die.

    It is assumed that the user already tried the Flash Integration via the steps mentioned here - https://software-dl.ti.com/mcu-plus-sdk/esd/AM243X/latest/exports/docs/api_guide_am243x/CUSTOM_FLASH_SUPPORT_GUIDE.html

    This FAQ walks you through the integration of MX25U51245GXDI00 (Macronix flash) which is not part of TI's EVM to emulate an experience of Custom Flash Integration.

    Integrating the Flash with 1s-1s-1s mode (Standard Read/SPI)

    1s-1s-1s mode is the simplest step one should start with. It has least amount of variables that impact the flash functioning.

    Fill the following items in the syscfg of the ospi_io example

    Changes in the OSPI

    • Set the Input Clock Frequency (Hz) to 200MHz i.e. 200000000 and Input Clock Divider as 8.
    • Disable the PHY

    Changes in the Flash

    • Configure the following items. These items are not suppose to change in any configuration (for majority of flashes)
    Configurable Items
    Block Erase CMD (3B)
    Block Erase CMD (4B)
    Chip Erase Command
    Flash Block Size In Bytes
    Flash Busy Timeout
    Flash JEDEC Device ID
    Flash JEDEC Manufacturer ID
    Flash Page Size In Bytes
    Flash Sector Size In Bytes
    Flash Size In Bytes
    Page Program Timeout
    Read Status Register CMD
    Sector Erase CMD (3B)
    Sector Erase CMD (4B)
    WEL Bit
    WIP Bit
    Write Enable CMD
    Write/Page Program Command
      • Set the Read Command as 0x3 (Usually standard)
      • Dummy cycles for CMD/DATA and all the other items should be 0 as not required.
      • Set Quirks Function as NULL.

      Rebuild the Test Application of OSPI IO with these changes. Make sure to keep the BOOT MODE as DEV-BOOT MODE for these type of tests. If this does not work recheck the configurations with the datasheet or SFDP table. If every thing is OK with the SW, recheck the HW.

      Integrating the Flash with 1s-1s-1s mode (Fast Read)

      These changes are in difference with the Previous step and in assumption that the previous steps have worked for 1s-1s-1s standard read.

      Changes in OSPI - NOT REQUIRED.

      Changes in the Flash

      • The read command changes from 0x3 to 0xB. Also the read is a fast read, hence the dummy cycles are required.
      • Set the Dummy Cycles (READ) as 10 (as per the datasheet)

      • Also the user must configure the Dummy Cycle Configuration in SYSCFG

      Note that the Configuration is only supported to write 1B(8bit) register only. If data to be written is > 8bits, this requires changes in the Flash Driver.

      For MX25U51245GXDI00, the Write register writes 2B at a time, so this requires re-writing the driver to support the same like this (function name Flash_norOspiSetRegCfg)

      Rebuild the Test Application of OSPI IO with these changes. Make sure to keep the BOOT MODE as DEV-BOOT MODE for these type of tests. If this does not work recheck the configurations with the datasheet or SFDP table.

      Integrating the Flash with 1s-1s-4s mode (Quad Read/QSPI mode)

      • Change the Protocol to 1s-1s-4s
      • Change the Read Cmd to 0x6B
      • Change the QE bit set sequence. This is must required based on the Flash Datasheet and supported mode as per the details mentioned.

      Details on QE bit as given in the syscfg information (?) -

      Rebuild the Application Test the application of OSPI_IO with these changes. If this does not work recheck the configurations with the datasheet or SFDP table. If every thing is OK with the SW, recheck the HW.

      Integrating the Flash with 4s-4s-4s mode (Quad Read/QPI mode)

      • Change the Protocol to 4s-4s-4s
      • Change the Read Cmd to 0xEB
      • Configure the QPI sequence based on the flash datasheet. This depends on the flash as well, some flash might not require this.

      Details on QPI Sequence as given in the syscfg information (?)

      Rebuild the Test Application of OSPI_IO with these changes. If this does not work recheck the configurations with the datasheet or SFDP table.

      Integrating the Flash with 4s-4d-4d mode (Quad Read/QPI mode DTR)

      • Change the Protocol to 4s-4d-4d
      • Change the Read Cmd to 0xED
      • Configure the STR/DTR Sequence. For this flash part the configuration is not required, hence can be skipped.

      Rebuild the Test Application of OSPI_IO with these changes. If this does not work recheck the configurations with the datasheet or SFDP table.


      This is the maximum configuration supported by this Flash but here are some tips for higher configurations

      Integrating the Flash with 1s-1s-8s mode (Octal Read/OSPI mode)

      To be done After 1s-1s-4s mode.

      • Change the Protocol to 1s-1s-8s
      • Change the Read Cmd (depends on the flash part, check the datasheet)
      • Configure the Octal Enable Type (depends on the flash part, check the datasheet)

      Details on Octal Enable Bit as given in the syscfg information (?)

      Integrating the Flash with 8s-8s-8s mode (Octal Read/OPI mode STR)

      To be done After 1s-1s-8s mode.

      • Change the Protocol to 8s-8s-8s
      • Change the Read Cmd (depends on the flash part, check the datasheet)
      • Configure the OPI Enable Sequence (depends on the flash part, check the datasheet)

      Details on OPI Sequence as given in the syscfg information (?)

      Integrating the Flash with 8d-8d-8d mode (Octal Read/OPI mode DTR)

      To be done After 4s-4s-4d mode.

      • Change the Protocol to 8d-8d-8d
      • Change the Read Cmd (depends on the flash part, check the datasheet)
      • Configure the Octal Enable Type (depends on the flash part, check the datasheet)
      • Configure the OPI Enable Sequence (depends on the flash part, check the datasheet)
      • Check if dummy clocks for CMD as well.

      Details on Octal Enable Bit as given in the syscfg information (?)

      Details on OPI Sequence as given in the syscfg information (?)

      Some Queries -

      Q. When should PHY be enabled ?

      A. PHY should not be enabled till the operating frequency for DTR <= 25MHz and STR <= 50MHz. Also the PHY configuration provided by SDK is only optimum for 8d-8d-8d (for Cypress Flash on the EVM), hence is suggested to kept disabled.

      Q. What if the protocol, user needs to run is not part of SYSCFG ?

      A. This needs the driver to be re-written by the user as this protocol is not a standard protocol. However, it might be supported by the Hardware, SDK might not support it out of the box due to its complexity and specific implementation.

      Q. What is the maximum frequency supported by the Hardware ?

      A. With PHY enabled, the maximum frequency supported is 200MHz. However it is suggested to keep the operating frequency as 133MHz to sustain at all PVT values.

      Q. How to configure the divider if the PHY is enabled ?

      A. When the PHY is enabled, the divider values are ignored.

      Q. What if the read values are not matching with the ones written ?

      A. Check the Dummy Cycles values. Sometimes the dummy cycle values may be a little bit different from the one mentioned in the datasheet. Also if there is still data misalignment then user might have to call OSPI_setRdDataCaptureDelay API after the Flash_open().