Part Number: AM2634-Q1
High Prio :
MCAL version : MCAL_AM263x_09.00.01.01
We are triggering Adc_StartGroupConversion for ADC channel groups, mapped for ADC SW trigger, cyclically at every 5ms, as in the screen below.

We see that the ADC result buffers do not show us an updated ADC conversion result for any of the channels mapped to the ADC group triggered by the SW trigger.
I am monitoring ADC0_1 to which I vary the Voltage inputs. ADC0_1 is the 1st channel in the group of 4 ADC channels which is mapped for SW trigger.

I can only see the updated voltage value in the next ignition cycle once i reset the ecu.
Test on LP eval board.
Temporary fix : He have currently changed all the SW triggered groups to be triggered as HW triggered groups based on EPWM0_A.
motor spinning tests are blocked due to the improper ADC conversion results.