This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
High Prio :
MCAL version : MCAL_AM263x_09.00.01.01
As per the config below, we have designed to trigger the ADC channel group SOC based on EPWM0_A.
We observe that when the PWM duty cycle is set to 0% duty cycle (0 count), the ADC conversion for this group is not happening even when the Voltage values on this ADC channel is changing in the current ignition cycle.
However, when we change the duty cycle back to 50%; the group conversion values are resumed and we can see the conversion results on the result buffer.
Temporary fix : No fix currently
motor spinning tests are blocked due to the improper ADC conversion results.
Hey Ashish,
As we discussed on the call, we are looking into implementing the workaround for getting this done in subsequent releases.
Regards,
Akshit