Part Number: LP-AM243
Hello all,
I'm unable to debug with the script load_dmsc_hsfs.
Sometimes I get the behaviour which is described in the related post, and it seems to load the sciclient initialization SBL.
But also sometimes it doesn'? What is going on? I'm using the same GEL files, the same sci client, the same scripts.
The only thing I alterated was the SBL itself, changing the version to debug instead of release using the example.
```
Connecting to MCU Cortex_R5_0!
Writing While(1) for R5F
Running the board configuration initialization from R5! //Gets stuck here, no more console log, no loading of app
com.ti.debug.engine.scripting.Target.run(): Timed out after 20000ms (C:\ti\mcu_plus_sdk_am64x_09_01_00_41\tools\ccs_load\am64x\load_dmsc_hsfs.js#117)
```
Regards,
Isaac Yuki