This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2634: Register Addendum and Database File for LOCK_STEP Info Could Be Wrong

Part Number: AM2634

Hello,

Question 1:

The TRM says:

a) "By default, after a device reset, both R5SS0 and R5SS1 are in lockstep."

b) "LOCK_STEP = 0 indicates the corresponding R5SS is in dual core mode, and LOCK_STEP = 1 indicates the corresponding R5SS is in lockstep mode."

The register addendum says:

c) The reset value of LOCK_STEP is 0:

How can statements a) and b) both be correct if statement c) is true? I think that the Reset value of bit field LOCK_STEP must be 1h.

Question 2:

When the value of the register MSS_CTRL_MMR (0x50D0 002Ch) is 0x00000101, bits 0 (MEMSWAP) and and 8 (LOCK_STEP) are set but the debugger shows LOCK_STEP is '0':

Why does the Register View not show LOCK_STEP = 1 please?

  • a) "By default, after a device reset, both R5SS0 and R5SS1 are in lockstep."

    After boot-up, it depends on the device initialization in SDL. If the LOCK_STEP of MSS_R5SSx_STATUS_REG is 0x1, the R5SSx is in lockstep mode, otherwise it is in dual-core mode.

    Why does the Register View not show LOCK_STEP = 1 please?

    The value in memory browser and register view should be consistent. Please refresh the contents of both windows 

  • After boot-up, it depends on the device initialization in SDL.

    What is the SDL please?

    The value in memory browser and register view should be consistent.

    Quite. The question is why aren't they.

    Update: Now I found the cause. The register definition (MSS_CTRL_MSS_CTRL.xml) contains a bug. The width element shown below is too small to capture Bit 8.

    If this is increased to 16 then LOCK_STEP == 1. Ditto 'MSS_CTRL_R5SS1_STATUS_REG'.

    Please correct the register xml for AM263 in CCS 12.7.

  • Sorry for my typo. I mean your SBL (secondary bootloader). If GEL files are used, please check which mode your R5SS in.

    Update: Now I found the cause. The register definition (MSS_CTRL_MSS_CTRL.xml) contains a bug. The width element shown below is too small to capture Bit 8.

    Great! Thank you, Kier. I will file a update ticket.

  • Thank you.

    If GEL files are used, please check which mode your R5SS in.

    Yes, I'm using DevBoot with GEL files. So the only entities that could modify the LOCK_STEP flag from the silicon default are the RBL and GEL files.

    If I set the following in AM263x.gel...

    #define Enable_OnTarget_Connect 0

    ...then the GEL files will do nothing when the debug probe is connected.

    After connection LOCK_STEP == 1 so it cannot be the GEL files changing this state from 0 to 1.

    Are you saying it is the RBL modifying the LOCK_STEP value?

  • I think so. RBL run memory init, PBIST test, and select R5SS operating mode. 

  • I see, thank you.

    In any case, I think for the Reset column in the Register Addendum to be useful it needs to reflect the value of the register at the earliest point where the user application has the opportunity to modify it.

    Saying the Reset value of LOCK_STEP = 0 is largely irrelevant if the end user only ever sees LOCK_STEP = 1 after POR due RBL.

    I'll raise a document feedback submission instead.

  • Hi Kier,

    My understanding is that the value in "reset" column of register field description is the default value after PORz is de-asserted and before the RBL is executed.

  • Hi QJ,

    If that is true then the Reset column is useless to the end user.

    Only a 'Post RBL' column is useful to the end user.