This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507: I2C Master Controller Multiple Data (more the 8 bytes) Transfer Polling Example

Part Number: MSPM0G3507

Hi, I am quite new to TI's MSPM0G3 series MCU and abit confused about transmitting mutliple bytes (more the max number of 8 TXFIFO) data in I2C Master Controller mode with polling method. Is there any example that I can refer to for this case?

  • Hi, 

    1. i2c_controller_rw_multibyte_fifo_interrupts

        This code example handle 16 bytes and 8 TXFIFOs very well.

        You can have a look.

    2. i2c_controller_rw_multibyte_fifo_poll

        Base on this example, add some code to be compatible with multi-byte(> 8) sending function.

        Just add some code after SYSCFG_DL_init(); of i2c_controller_rw_multibyte_fifo_poll.c

        I didn't test this code, bug logic should be correct.

       

        SYSCFG_DL_init();
    
        /* Set LED to indicate start of transfer */
        DL_GPIO_setPins(GPIO_LEDS_PORT, GPIO_LEDS_USER_LED_1_PIN);
    
        gTxLen = I2C_TX_PACKET_SIZE;
    
        /*
         * Fill the FIFO
         *  The FIFO is 8-bytes deep, and this function will return number
         *  of bytes written to FIFO */
        gTxCount = DL_I2C_fillControllerTXFIFO(I2C_INST, &gTxPacket[0], gTxLen);
    
        /* Wait for I2C to be Idle */
        while (!(
            DL_I2C_getControllerStatus(I2C_INST) & DL_I2C_CONTROLLER_STATUS_IDLE))
            ;
    
        /* Send the packet to the controller.
         * This function will send Start + Stop automatically.
         */
        DL_I2C_startControllerTransfer(I2C_INST, I2C_TARGET_ADDRESS,
            DL_I2C_CONTROLLER_DIRECTION_TX, gTxLen);
    
        while (gTxCount < gTxLen) {
            //Waiting for txfifo empty
            while (!(DL_I2C_getRawInterruptStatus(I2C_INST) & DL_I2C_INTERRUPT_CONTROLLER_TXFIFO_EMPTY));
            //clear interrupt
            DL_I2C_clearInterruptStatus(I2C_INST, DL_I2C_INTERRUPT_CONTROLLER_TXFIFO_EMPTY);
            //Write more data to I2C FIFO
            gTxCount += DL_I2C_fillControllerTXFIFO(I2C_INST, &gTxPacket[gTxCount], gTxLen - gTxCount);
        }
    
        /* Poll until the Controller writes all bytes */
        while (DL_I2C_getControllerStatus(I2C_INST) &
               DL_I2C_CONTROLLER_STATUS_BUSY_BUS)
            ;
    
        /* Trap if there was an error */
        if (DL_I2C_getControllerStatus(I2C_INST) &
            DL_I2C_CONTROLLER_STATUS_ERROR) {
            /* LED will remain high if there is an error */
            __BKPT(0);
        }
    
        /* Wait for I2C to be Idle */
        while (!(
            DL_I2C_getControllerStatus(I2C_INST) & DL_I2C_CONTROLLER_STATUS_IDLE))
            ;
    
        /* Add delay between transfers */
        delay_cycles(1000);

    Regards,

    Helic

  • Thanks so much Helic..