Part Number: EK-TM4C123GXL
Hello,
in the following of the work done in this THREAD I now have this code inside the adc interrupt handler :
switch(ADCComparatorIntStatus(ADC0_BASE)){
case 0x00000001: //CMP0
ADC_FLAG_1=0x01;
Semaphore_post(S_Handle_UnlockSEND);
GPIO_toggle(Board_LED2);
break;
case 0x00000002: //CMP1
ADC_FLAG_1=0x02;
Semaphore_post(S_Handle_UnlockSEND);
GPIO_toggle(Board_LED1); //just for debug
break;
case 0x00000003: //CMP1
ADC_FLAG_1=0x03;
Semaphore_post(S_Handle_UnlockSEND);
GPIO_toggle(Board_LED0); //just for debug
break;
default :
break;
}
ADCComparatorIntClear(ADC0_BASE, 0x000000ff);
//TimerIntClear(TIMER2_BASE, TIMER_TIMA_TIMEOUT); // must clear timer flag FROM timer
ADCIntClear(ADC0_BASE,0);
But aparently the Semaphore_post() causes the program to crash. Is it because i am mixing TIRTOS with TIVAWARE ?