Part Number: AM2634
Hi Ti,
Could you please help answer the following questions?
How to optimize secure boot on AM2634 to reduce the secure boot time?
The current test information is as follows:
DEVICE TYPE: HS-SE
SDK version: mcu_plus_sdk_am263x_09_01_00_41-windows-x64
tifs version: tifs_am263x_09_01_00_03-windows-x64
SBL size is 350KB, APP size is 1100KB, TIFS size is 117KB. The test secure boot time under these conditions is around 1 second.
The current confirmation mainly consumes time in the signature verification interface of the APP, Bootloader_verifyMulticoreImage->Bootloader_socAuthImage.
This issue is quite urgent, please help resolve it as soon as possible.
thanks.